Select your country/region in the menu or by clicking on the world map *
Country Selector Alternate Image

Back-up Power Connection -  Stab-lok Loadcentre Retrofit Generator Panels




This panel offers up to 20 circuits that can be used to operate critical loads such as heating, lights, pumps and refrigeration in emergency situations. The panel is factory wired for use with a bonded neutral generator, but for flexibility, simply field modification allows this panel to be used with unbonded neutral generators as well.

Stab-lok Retrofit Generator Panels can be connected via a subfeed breaker from any main breaker loadcentre.

To know more

To learn more about 

  • Overview
    • Description
  • Downloads
    • Documents
  • Support
    • Contact Us