Technical FAQs

Ask a Question

What quantity and size of conductors can be used on a SN1000MA neutral assembly?

Product Line:
Circuit Breaker Enclosure

Resolution:
The SN1000MA accepts (3) #3/0 AWG - 500 kcmil aluminum or copper conductors in and out. The service grounding lug accepts (1) #1 - 4/0 AWG aluminum or copper conductor.
 
Was this helpful?
What can we do to improve the information ?