Technical FAQs

Ask a Question

What are the part numbers for the field installable red pilot lights for use in NEMA 1 enclosed 2510M and 2510T devices?

Issue:
What are the part numbers for the field installable red pilot lights for use in NEMA 1 enclosed 2510M and 2510T devices?

Product Line:
NEMA Contactors and Starters

Environment:
Product selection

Cause:
Product selection

Resolution:
9999MP1 is 110-120v
9999MP2 is 208-240v
9999MP3 is 440-600v


CTA-ID : 2049751
Was this helpful?
What can we do to improve the information ?