Technical FAQs

Ask a Question

What are the dimensions for the Q23225NF and Q23225NS circuit breaker enclosures?

Issue:
Dimensions

Product Line:
Q2 Circuit Breaker Enclosure

Cause:
Product dimensions

Resolution:
The enclosure is 26.12" H x 9.62" W x 4.75" D.
The Q23225NS surface mount cover is the same height and width as the enclosure.
The Q23225NF flush mount cover is 27.62" H x 11.12" W. 


CTA-ID : 2004016
Was this helpful?
What can we do to improve the information ?