Technical FAQs

Ask a Question

What is suffix 2307 on an FAL 3 pole breaker?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Suffix 2307 consisted of a 1A 1B aux contacts, 120 volt shunt trip and a handle padlock assembly. Or, order as an FA frame breaker with suffix 1380 and install the HPAFK padlock attachment in the field.


CTA-ID : 2004314
Was this helpful?
What can we do to improve the information ?