Technical FAQs

Ask a Question

What size DIN rail is required for track mounting an 8910 DPA contactor?

The 8910 DPA 20A through 60A contactors can be installed onto 35mm DIN rail and requires the use of the 9999 DMB1 mounting bracket. The 75A through 352A are panel mounted.

CTA-ID : 2004881
Was this helpful?
What can we do to improve the information ?