Technical FAQs

Ask a Question

What are the coordinated short circuit options for the 8903SM lighting contactor?

100,000 amps rms 480 volt maximum when using Square D 40 amp current limiting circuit breaker part number IFL34040

100,000 amps rms 600 volt maximum when using Class RK5 30 amp current limiting fuses having interrupting rating not less than 100,000 amps.

10,00 amps rms 480 volt maximum when using 40 amp UL Listed thermal magnetic inverse time circuit breaker with interrupting rating not less than 10,000 amps.

5,000 amps rms 600 volt maximum when using 40 amp UL Listed thermal magnetic inverse time circuit breaker with interrupting rating not less than 5,000 amps.
Was this helpful?
What can we do to improve the information ?