Technical FAQs

Ask a Question

What is the coil consumption of the 8903 Type L lighting contactor with DC coil; Form Y48?

The coil burden is as follows:
DC Volts Inrush Amps Sealed Amps
24 8.000 0.727
32 8.000 0.593
48 6.000 0.361
115 2.255 0.144
230 1.080 0.072





CTA-ID : 2005714
Was this helpful?
What can we do to improve the information ?