Technical FAQs

Ask a Question

Who provides support for Class 8942 Pump products?

The 8942 Pump devices were used with sprinkler irrigation systems. They were obsoleted in the late 1970s and there is no direct replacement.

Users may be able to replace these devices with a combination starter package. The application and the user`s needs should be reviewed to determine if an alternative device is available.
Was this helpful?
What can we do to improve the information ?