Technical FAQs

Ask a Question

What is the UL Listed current rating of the TeSys Quickfit LAD34 power connection module?

It`s rated 25A when in a stand-alone application or when used with the TeSys power splitter boxes. It`s rated 16A when used with the TeSys power & control splitter boxes.


CTA-ID : 2005725
Was this helpful?
What can we do to improve the information ?