Technical FAQs

Ask a Question

Do we make an 800 amp current limiting circuit breaker?<br />

Issue:
Do we offer a 800a current limiting circuit breaker ?

Product Line:
Molded case circuit breakers

Environment:
Distribution equipment

Cause:
Need a 800a current limiting breaker

Resolution:
600 amps is the maximum we offer.
The Schneider Electric current  limiting breaker now available in North America are the Powerpact
HJ/HL/HR, JJ/JL/JR, and LJ/LL/LR frame circuit breakers


 

Was this helpful?
What can we do to improve the information ?