Technical FAQs

Ask a Question

Are NEMA Type 1 Heavy Duty safety switches available without knockouts?

Issue:
Product Features

Product Line:
HD SS

Cause:
Clarification of knockouts

Resolution:
NEMA Type 1 Heavy Duty safety switches, 30 through 200 ampere, will be provided with knockouts. They are not available without knockouts. For an enclosure without knockouts, consider using a NEMA Type 12 Heavy Duty safety switch.
NEMA Type 1 Heavy Duty safety switches, 400 through 1200 ampere are not provided with knockouts. 


CTA-ID : 2005514
Was this helpful?
What can we do to improve the information ?