Technical FAQs

Ask a Question

Do we have lugs for an LAL breaker which will accept 2-350kcmil conductors?

Product Line:
Legacy Circuit Breaker

Environment:
Electrical Distribution Equipment

Resolution:
We do not offer a mechanical lug option. Maximum size for (2) conductors is 250 kcmil for Mechanical Lug.
However, the optional compression lug kit VC400LA35 will accept (2) 250kcmil to 350kcmil.
 
Was this helpful?
What can we do to improve the information ?