Technical FAQs

Ask a Question

What is a HU361AWKEI4M safety switch?

Issue:
Identification

Product Line:
Heavy Duty Safety Switch

Environment:
Identification

Cause:
Clarification

Resolution:
This device consists of a HU361AWK safety switch with an EIK034M (2-NO/2-NC contacts) Electrical Interlock Kit factory installed. The EIK034M could be field installed in any HU361, HU361RB, HU361DS, HU361A or HU361AWK, Series F design of safety switch.


CTA-ID : 2006481
Was this helpful?
What can we do to improve the information ?