Technical FAQs

Ask a Question

Can an I-Line panel be supplied with a PowerPact breaker that has an adjustable trip setting?

Issue:
Can an I-Line panel be supplied with a PowerPact breaker that has an adjustable trip setting?

Product Line:
PowerPact H, J, L, P, R frame electronic trip breakers

Environment:
All I-Line electronic trip PowerPact breakers with the exception of those with the Basic ET 1.0I trip unit are included.

Cause:
Can I-Line electronic trip PowerPact breakers be installed in I-Line panels?

Resolution:
All I-Line electronic trip PowerPact breakers with the exception of those with the Basic ET 1.0I trip unit have adjustable trip settings. However, HCN and HCM I-Line panel wireway covers do not allow the trip unit to be seen when closed.
HCP, HCP-SU, HCR-U wireway covers have been modified to allow the trip unit to show.



CTA-ID : 2006300
Was this helpful?
What can we do to improve the information ?