Technical FAQs

Ask a Question

What is the lug wire range of a QOM1-VH?

Product Line:
QOM1-VH Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The wire range is 1 - #12 - 2/0 per phase. aluminum or copper.


CTA-ID : 2006632
Was this helpful?
What can we do to improve the information ?