Technical FAQs

Ask a Question

What are the ratings of the Masterpact NW standard and low-level auxiliary contacts?

Inquiry:
For Masterpact Aux. switches, please explain what is meant by ``Standard 10mA/24V minimum load `` and ``Low Level   1mA/4V minimum load``
What are the ratings of the Masterpact NW standard and low-level auxiliary contacts?

Product Line:
Masterpact NW

Resolution:
This means that the standard switch will not reliably operate at less than 24V and 10mA, and the Low Level switch will not operate reliably at less than 1mA and 4V.
The maximum current at specific voltages is specified in the table below.



 
Was this helpful?
What can we do to improve the information ?