Technical FAQs

Ask a Question

Is the QO120K switch duty rated?

Issue:
Some QO single pole breakers are SWD (switch duty) rated. Does that include the version of those breakers that are key operated, such as the QO120K?

Product Line:
Circuit Breakers

Environment:
Applies to QO-K key operated breakers.

Cause:
SWD rating for QO breakers

Resolution:
No, the QO-K key operated circuit beakers are not SWD rated.

For a list of circuit breakers that have the SWD switch duty rating, see FAQ number FA91402.
Was this helpful?
What can we do to improve the information ?