Technical FAQs

Ask a Question

What is the cross reference for a QMB362T21?

Issue:
Cross reference

Product Line:
QMB

Cause:
Selection by cross reference

Resolution:
The QMB362T21 is a Series D2, 30 ampere/60 ampere switch. It is obsolete with no direct replacement. An option would be to order a QMB362T that has (2) 60 ampere twin switches and a QMB361T that has (2) 30 ampere twin switches. An additional 4.5`` of mounting space would be required for this option.


CTA-ID : 2006796
Was this helpful?
What can we do to improve the information ?