Technical FAQs

Ask a Question

What is the replacement 240 volt coil for a Type SD NEMA Size 2 contactor or starter?

Product Line:
 
NEMA style type S Contactors and Starters

Resolution:
 
For 2 & 3 pole devices 31063-409-47 for 60 hertz or 31063-409-48 for 50 hertz. For 4 & 5 pole devices 31063-400-47 for 60 hertz 0r 31063-400-48 for 50 hertz.


CTA-ID : 4770
Was this helpful?
What can we do to improve the information ?