Technical FAQs

Ask a Question

Can two LC1K0610 be used to replace an LC2K0610 reversing contactor?

Product Line:
Tesys K Line Contactors
Since the mechanical interlock is internal and is not available as a spare part, it is not possible to build an LC2K reversjing contactor from (2) LC1K non-reversing contactors.

CTA-ID : 2007539
Was this helpful?
What can we do to improve the information ?