Technical FAQs

Ask a Question

What does the RB suffix of a QO load center catalog number indicate?

Issue:
Product design feature

Product Line:
QO load centers

Environment:
Catalog logic

Resolution:

NEMA 3R QO load centers with a RB suffix in the catalog number will have a hub opening in the top endwall. It will accept 3/4" through 2 1/2" B type hubs. The hub opening is covered with a closing cap (BCAP). Hubs are ordered separately.


CTA-ID : 2007410
Was this helpful?
What can we do to improve the information ?