Technical FAQs

Ask a Question

When cross-referencing an ASCO mechanically held lighting contactor, what is Square D equivalent to 47* module option?<br /><br />* Could represent 47D, 47E, 47F or 47G.

This is a solid state 2-wire control module which provides the same function as the Squared D factory modification Form R6. The 47 will be followed by a letter which indicates the control voltage as listed below:

D = 120 volt 60 hertz; Square D voltage code V02.
E = 24 volt 60 hertz; Square D voltage code V01.
F = 24 volt DC, Not offered by Square D.
G = 277 volt 60 hertz.


CTA-ID : 2008183
Was this helpful?
What can we do to improve the information ?