Technical FAQs

Ask a Question

Can 2 dissimilar TeSys contactors be mechanically interlocked together?<br /><br /><br /><br />

If the 2 are physically the same size a mechanical interlock may fit, HOWEVER, the carrier speeds of the contactors may be different and not allow the contacts to open/close at the same time. This is not a test proven combination and is not recommended.


CTA-ID : 2007796
Was this helpful?
What can we do to improve the information ?