Technical FAQs

Ask a Question

Are Square D Heavy Duty Safety Switches tested for seismic applications?

Issue:
Application

Product Line:
Heavy Duty Safety Switches

Environment:
Application

Cause:
Clarification

Resolution:
Yes, Square D Heavy Duty Safety Switches have been tested and self certified for seismic applications. SEE EXCEPTIONS BELOW.
EXCEPTIONS: 1000Vdc Photovoltaic Switches (REHU Prefix), Fiberglass Reinforced Polyester Type 4X Switches (DF or DX Suffix) and Type 7/9 Enclosed Molded Case Switches (H60XFA, H60XFA1212, H100XFA, H100XFA1212, H225XJG, H225XJGAA).  


CTA-ID : 2007994
Was this helpful?
What can we do to improve the information ?