Technical FAQs

Ask a Question

What are the contact ratings of the 9001 BG***, BW***, and BR*** control stations?

 
Product Line:
9001BG, 9001BW, 9001BR, control stations, 30MM

Environment:
9001 Control Stations

Resolution:
They are rated NEMA B600 for AC and NEMA P600 for DC. This is 5 amps continuous and 600 volts maximum. They don`t have horsepower ratings so they are not rated for direct motor starting duty.
 
CTA-ID : 2007833
Was this helpful?
What can we do to improve the information ?