Technical FAQs

Ask a Question

Does the QMB324 Series D2 switches include the Rail Extensions?

Issue:
Product Design Features

Product Line:
QMB Branch Switches

Environment:
Switch Components

Cause:
Installation

Resolution:
Yes, the rail extensions are included with the QMB324 Series D2 switches..


CTA-ID : 2008055
Was this helpful?
What can we do to improve the information ?