Technical FAQs

Ask a Question

M30H13F----what is this?

``M30`` is the older style Masterpact, IEC rated, 3000 amp. ``H1`` is the interrupting level, ``3`` if for 3-pole, and ``F`` means that it is a fixed breaker.


CTA-ID : 2008312
Was this helpful?
What can we do to improve the information ?