Technical FAQs

Ask a Question

What is the difference between the feature and base unit solid state overload relays?

Product Line:
 
NEMA style Overload Relays

Resolution:
 The feature unit provides the following additional functionality:
1. Selectable trip class
2. Class II ground fault detection
3. Accepts the Analog Output Module




CTA-ID : 2008567
Was this helpful?
What can we do to improve the information ?