Technical FAQs

Ask a Question

What Equipment Ground Kit is used with the DT363, Series F05, Double Throw Safety Switch?

Issue:
Product Design Features

Product Line:
Double Throw Safety Switches

Environment:
Equipment ground kit

Cause:
application

Resolution:

The Equipment Ground Kit is factory installed in this device. Three lugs are provided, each accepting (1) #12 - 1/0 AWG aluminum or (1) #14 - 1/0 copper ground conductor.

 
Was this helpful?
What can we do to improve the information ?