Technical FAQs

Ask a Question

Can the time delay on a GC100 ground-fault relay be adjusted?

Issue:
Can the time delay on a GC100 ground-fault relay be adjusted?

Product Line:
GC100 ground fault relay

Environment:

Cause:

Resolution:
Yes. There are four (4) time delays (0.10, 0.20, 0.30 and 0.50 second) settings. Higher settings may help ride through spikes.  The time delay adjustment are inside the relay under the cover.  See attached photo.


CTA-ID : 2009508
Was this helpful?
What can we do to improve the information ?