Technical FAQs

Ask a Question

What are the dimensions of the 2601 Type A and Type B drum switch mounting holes?

The back of these units have 4 oval mounting holes. The Type A are 3/16`` x 9/32``. The Type B are 9/32`` x 3/8``.


CTA-ID : 2009507
Was this helpful?
What can we do to improve the information ?