Technical FAQs

Ask a Question

What is the correct range for W4062 which is where LCR can be monitered via serial communication?

There is a typo on page 27 of the ATS46 Communication Option manual ( VD0C32S303A )  

The manual shows the range of W4062, LCR ( Motor Current ) to be 0 - 999.  
The actual range is 0-65535.



CTA-ID : 2009302
Was this helpful?
What can we do to improve the information ?