Technical FAQs

Ask a Question

Is the 8910 DP42 CSA Certified or UL Listed?

No, it is not. For a 40 amp, 2-pole CSA Certified or UL Recognized definite purpose contactor, use an 8910 DPA42. For a UL Listed contactor, add form U1 to the contactor catalog number.


CTA-ID : 2009147
Was this helpful?
What can we do to improve the information ?