Technical FAQs

Ask a Question

Will the LA4DC1U diode suppression unit fit onto the Tesys DC controlled contactor?

Will the LA4DC1U fir on a Tesys D contactor with DC coil

Product Line:
IEC contactors and starters

Products sold and used in the United States

Identifying product compatibility

No. The LA4DC1U diode unit will only fit the pre-TeSys contactors but since the TeSys DC controlled LC1D09 - D38 contactors include suppression automatically, it`s not needed.

CTA-ID : 2009392
Was this helpful?
What can we do to improve the information ?