Technical FAQs

Ask a Question

Can the GS1 fusible IEC switches be used on DC voltage?

Yes, they are rated up to 250 volts DC.


CTA-ID : 2009410
Was this helpful?
What can we do to improve the information ?