Technical FAQs

Ask a Question

What is form Y91 or Y1072 when used with the fusible combination starters?

Product Line:

Type S combination starters
 
Resolution:
 
Form Y91 allows substitution Class J fuse clips in place of standard clips. This is a no charge option.

Note: Form is OBSOLETE in the United States However it is still a valid option for the Canadian Market. If Class J is desired in the United States use Form Y1072.



CTA-ID : 2005540
Was this helpful?
What can we do to improve the information ?