Technical FAQs

Ask a Question

What are the mechanical lugs for a LC1F115 ?

Use a DZ2FF6 kit of 6 lugs. If using a direct-mounted overload relay, use (3) DZ2FF1 (kit of 1 lug) on the line side of the contactor and (3) DZ2FG1 (kit of 1 lug) on the load side of the overload relay.


CTA-ID : 2005883
Was this helpful?
What can we do to improve the information ?