Technical FAQs

Ask a Question

What is the voltage code suffix to order an 8536 SAO12 with a 380V 50Hz coil?

A 380V 50Hz coil is not available on the size 00 contactor or starter. Use a size 0 starter to get a 50HZ coil at 380V. The voltage code suffix is V05. Ex: 8536SBO2V05


CTA-ID : 2004965
Was this helpful?
What can we do to improve the information ?