Technical FAQs

Ask a Question

What circuit breaker enclosure will accept a KAL or KHL circuit breaker?

Issue:
Product Design Features

Product line:
Circuit breaker enclosures

Cause:
application

Resolution:
ALL THE KA ENCLOSURES ARE OBSOLETE, NO LONGER AVAILABLE, WITH NO DIRECT REPLACEMENT. NEED TO CONSIDER THE PowerPact J Frame breakers with J Enclosures.

The KHL circuit breakers(225Amp Maximum) were used in the following enclosures:
1) KA225F (NEMA 1, flush mount applications).
2) KA225S (NEMA 1, surface mount applications).
3) KA225RB (NEMA 3R applications).
4) KA225DS (NEMA 1, 3, 3R, 4, 4X, 5 or 12 applications).
5) KA225A (NEMA 12K application).
6) KA225AWK (NEMA 1, 3R, 5 or 12 applications).
7) KA225X (NEMA 7 applications).
8) KA225Y (NEMA 9 applications).
NOTE: The KHL circuit breaker (250 AMPERE MAXIMUM) can also be mounted in the PREVIOUS Series enclosures, BUT ONLY if marked on the wiring diagrams, LA400F (NEMA 1, flush mount applications), LA400S (NEMA 1, surface mount applications), LA400R (NEMA 3R applications), IK250DS (NEMA 1, 3, 3R, 4, 4X, 5 or 12 applications), or IK250AWK (NEMA 1, 3R, 5 or 12 applications).
Was this helpful?
What can we do to improve the information ?