Technical FAQs

Ask a Question

What is the difference between the HU361A and HU361-2A?

Issue:
Product Design

Product Line:
HD SS

Cause:
Clarification

Resolution:
These switches are electrically equivalent (3 pole, 30A, 600V, non fused, NEMA Type 12K), however, the HU361-2A is in a larger (60A size) enclosure.


CTA-ID : 2009488
Was this helpful?
What can we do to improve the information ?