Technical FAQs

Ask a Question

What is the part number for the current measurement board for the ATS46 softstarter?


Issue: Current measurement board part number
Environment: Replacement parts
Cause: current measurement board failure.
Resolution: See attached document for the current measurement board part numbers. Note: The current measurement boards for all ATS46 models are obsolete and no longer available. The ATS46 softstarter should be replaced with the current version of ATS48.
Was this helpful?
What can we do to improve the information ?