Technical FAQs

Ask a Question

What would cause the ATS46 to go out on overcurrent?

The Fault code is OcF:
Possible Causes are:
 * High impedance short circuit at the output of the controller
 * Internal short circuit
 * Improper sequence of shorting contactor

Possible Corrective action:
Remove power from unit and check for:
-Damage to power cables and/or motor insulation
-Damage to thyristors
-Damage to shorting contactor/contactor stuck in closed position

If none of the obvious is seen then
-- identify exactly when the fault is occurring in relation to startup
-- identify what In, ILt and acceleration are set for
-- identify what is the full load amperage of motor
-- and determine the currents being pulled in the LCR parameter of starter.

After obtaining this information contact Schneider Electric Product Support for further assistance.
Was this helpful?
What can we do to improve the information ?