Technical FAQs

Ask a Question

Is there a two-pole QO feed thru breaker that is not a breaker? has no switch or tripping mechanism.

Issue:
Is there a two-pole QO feed thru breaker that is not a breaker?  has no switch or tripping mechanism.

Product Line:
QO

Environment:

Cause:

Resolution:
QO sub feed lug, like 60A QO60SL and 125A QO2125SL.


CTA-ID : 2010037
Was this helpful?
What can we do to improve the information ?