Technical FAQs

Ask a Question

What is the coil burden for a NEMA size 3 starter or contactor?

Issue:     
Identifying the coil consumption of a NEMA size 3 device

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Need to know the coil conumption of a NEMA size 3 device


Resolution:
700VA inrush, 46VA sealed


CTA-ID : 2009603
Was this helpful?
What can we do to improve the information ?