Technical FAQs

Ask a Question

Is a PK2MB retaining bracket required for use in a QO2100BNS enclosure if used as a main breaker?

Issue:
Product usage

Product Line:
QO Circuit Breaker Enclosures

Cause:
Installation

Resolution:
No the PK2MB retaining bracket, is not required. The incoming conductor are connected to the lugs of the mounting base. If the 2 pole breaker is removed from the base, the breaker load lugs will not be energized(or hot).


CTA-ID : 2009706
Was this helpful?
What can we do to improve the information ?