Technical FAQs

Ask a Question

What is the pinout for the remote keypad cable for an Altivar 58? <br />Customer would like to extend the cable.

A 50ft cable of the construction detailed below was tested for Electrical Fast Transient Burst Immunity and Radiated RF Immunity per IEC 1000-4 International Standards with the ATV58 and a keypad. The products passed testing. Cable lengths longer than 50 ft are not recommended.

The termination points for the ATV58 and the keypad are as follows:

Pin on ATV58 Designation Pin on keypad
3 Data A 3
4 0 VDC 4
6 10 VDC 6
7 Data B 7
D shell housing(sheild) Ground D shell housing (shield)

The cable must be shielded cable with 2 sets of 22AWG twisted pair conductors. (One pair for the 0 VDC and 10 VDC and the other for Data A and Data B.) The shield must terminate to the D-shell connector on both ends of the cable. No other pins should be connected.

CTA-ID : 2011348
Was this helpful?
What can we do to improve the information ?