Technical FAQs

Ask a Question

Is the Vario switch defeatable?

Product Line:
 
Vario UL508 Disconnect Switches
 
Resolution:
 
The question is is the handle defeatable? The answer is NO. This is a UL508 switch. Only UL98 switches are required to have defeatable handles.


CTA-ID : 2011124
Was this helpful?
What can we do to improve the information ?