Technical FAQs

Ask a Question

Is a 24VDC coil available for a 8903LX type contactor?

No it is not. It is only available for the electricaly held 8903L type contactor when Form Y48 is added to the catalog number.


CTA-ID : 2011134
Was this helpful?
What can we do to improve the information ?