Technical FAQs

Ask a Question

Do we offer any drives rated for 120v or 115v single phase operation that can run a 230vac three phase motor?

Issue:
Do we offer any drives rated for 120v or 115v single phase operation that can run a 230vac three phase motor?

Product Line:
Altivar ATV12

Environment:
All  with suffix F.

Cause:
Only has 120vac 1 phase input but needs to run a 3 phase motor.

Resolution:
Yes.

Some of the ATV12 units are rated for 115v single phase input.  

They are as follows:
ATV12H018F1 = .25hp / 1.4 amps
ATV12H037F1 = .5hp / 2.4 amps
ATV12H075F1= 1hp / 4.2 amps

CTA-ID : 2011141
Was this helpful?
What can we do to improve the information ?